Smart Switch - Quick Start Guide (Coming Soon)
Your HALO Home In-Wall Smart Switch allows you to turn ON and OFF standard lighting, exhaust and ceiling fans from your HALO Home App or other HALO Home accessories. In this Quick Start Guide you will:
I. Pair your installed HALO Home In-Wall Smart Switch to the HALO Home App.
II. Learn about additional features and information.
I. Pair Your In-Wall Smart Switch
1. Install the HALO Home In-Wall Smart Switch in your desired location
(See enclosed instruction sheet. For indoor use only. Only for use with standard lighting: incandescent max. 960W or CFL/LEDs max. 400W, or small motor loads: ½ HP Motor or 1800W (15A) resistive).
Once powered your HALO Home In-Wall Smart Switch will:
- turn ON the attached lighting load after a short delay
- flash the indicator LED to indicate that it is ready to be paired
Note: The HALO Home In-Wall Smart Switch operates as soon as power is applied and can be used to control the connected load before being paired with the HALO Home App.
2. Create your HALO Home Account
Download the HALO Home app and register >
Already a HALO Home user? Skip to the next step.
3. Add the Smart Switch to the app
IMPORTANT! iPhone 11 Users. Having issues? Please read this>
Note: Make sure your mobile device’s Bluetooth is turned on and within 40’ of the Smart Switch.
- Tap the " ☰" menu button.
- Navigate to "Devices" and tap the " + " icon.
(The app will scan for your installed, unpaired devices).
- Select the Smart Switch and click “Add” to complete the pairing process.
Once paired, the Smart Switch indicator LED will stop flashing.
Note: If the device firmware is outdated, an exclamation point will display on the device in the device list. Tap the exclamation point and following the onscreen instructions to update the device.
II. Additional HALO Home In-Wall Smart Switch Information
Now you can:
-
Add your device to a Group
-
Set up a Schedule
- Set up a Scene (Sets brightness and color temp where you need it.)
Override lighting manually (temporary)
The In-Wall Smart Switch will control the connected lighting regardless of connection to the HALO Home App or other HALO Home Controllers. Simply use the onboard switch to turn ON and OFF the connected load. The connected lighting will also respond to a manual power cycle, turning the connected load ON until it receives the next HALO Home App, accessory, or voice command.
Reset the HALO Home In-Wall Smart Switch to factory settings
ONLY DO THIS STEP IF YOU ARE UNABLE TO REMOVE THE DEVICE FROM THE APP.
If removal is not possible, delete it by clicking "my device is broken" and then do the factory reset steps:
To reset the HALO Home In-Wall Smart Switch to factory settings:
- Press and hold the ON button for 12 seconds to reset.
- The LED will start flashing indicating the reset is processing and will continue flashing to indicate that it is ready to be paired with the HALO Home App.
Power cycle behavior
- The HALO Home In-Wall Smart Switch will turn connected lighting ON if power is cycled