Smart Plug-in Lamp Dimmer - Quick Start Guide
1. LED will blink indicating the Lamp Dimmer is ready to be claimed by the mobile app.
- Ensure the LED indicator on your dimmer is illuminated
Note: Lamp Dimmer is for lamps only.
Note: Wattage maximum:
- 300W Incandescent
- 150W CFL/LED
Note: If you have already registered for a Halo Home account, you may skip to step 4.
2. Download the Halo Home App to your smart mobile device
3. Create a user account and validate via email
- Enter your email address as your user account name.
- Select a password of at least 8 characters from the mobile application "Register" screen.
- Verify identity by clicking the link in your validation email.
4. Add the Lamp Dimmer to the app
IMPORTANT! iPhone 11 Users. Having issues? Please read this>
- Press the "
" menu button in the upper left-hand corner and navigate to "Devices", then press the "+" button on the screen.
- Allow your device list to populate and select the Lamp Dimmer
Note: At least one HALO Home Lamp Dimmer (or compatible device) will need to be installed and powered in order to add it to the HALO Home App device list
- Press "Add". (It may take up to 30 seconds for the process to complete.)
5. Controlling without the Halo Home App
- The Lamp Dimmer may be controlled outside the Halo App with the ON/OFF button.
- Press the ON button to turn the light on and off.
- Press and hold the ON button to dim the lights down. The light will continue to dim until the button is released.
- The next time the ON button is pressed and held, the light will dim up until the button is released.
Note: Dimming capabilities only work when lamp is using a dimmable light bulb.
Creating a group
- Press the "
" menu button in the upper left-hand corner and navigate to “Groups”, then Press the “+” button on the screen.
- Choose a name for your group and click “Done”.
- Drag and drop your Smart Dimmer into the group to add all non-smart fixtures.
Note: All non-smart fixtures wired to your Smart Dimmer will be automatically included in the group.
Setting up a schedule
To set up a new schedule for a claimed device, follow these steps:
- Tap the "
" icon in the top left-hand corner
- Select the schedule tab and click the "+" to set up a schedule
- Name your schedule
- Set your desired time using the dial
- Tap the days of the week you want the schedule applied to
- Tap “Save” to apply your schedule
- Click the " ⋮ " symbol next to your schedule
- Click “Apply” to select the product you would like to include in the schedule
- “Save” to update and save your schedule
Reset to factory settings
ONLY DO THIS STEP IF YOU ARE UNABLE TO REMOVE THE DEVICE FROM THE APP.
If removal isn't possible, delete it by clicking "my device is broken" and then do the factory reset steps:
- Hold the ON button for 15 seconds to reset
Dimming
- The Lamp Dimmer will dim fixtures from 100% to 5% using the ON/OFF button as well as through the mobile app.
Manual override
- If the light is off in the app, cycle power one time, the light will return to the previous ON state.