Eaton Logo
Go back to HALO Home page

In-Wall Smart Dimmer

1. Install the In-Wall Smart Dimmer in your desired location (See enclosed instruction sheet)

  • Ensure the LED indicator is illuminated

Note:

  • Dimmer must be installed and wired to a circuit with dimmable standard light(s), in order to be used.
  • Indoor use only
  • Max 600W incandescent/300W LED or CFL
  • If you have already registered for a Halo Home account, you may skip to step 4
     

2. Download the Halo Home App to your smart mobile device

 

3. Create a user account and validate via email

  1. Enter your email address as your user account name
  2. Select a password of at least 8 characters from the mobile application "Register" screen
  3. Verify identity by clicking the link in your validation email

 

4. Add the Smart Dimmer switch to the app

  1. Tap the " ☰ " menu button in the upper left corner
  2. Navigate to "Devices" and tap the " + " icon
  3. Select the switch and press "Add". (It will take about 30 seconds for the process to complete.)
  4. You can now associate it to a device.

Note: Stay in range. Your mobile device will need to be within 40' of the device when pairing.

 

5. Create a group

  1. Press the " ☰ " menu button in the upper left corner
  2. Navigate to “Groups” and tap the + " icon
  3. Enter a unique name for your group and press “Done”
  4. Drag and drop devices to the top area to add them to the group

Note: All standard fixtures connected to the Smart Dimmer circuit will be automatically included in the group

 

6.Reset to Factory Settings

ONLY DO THIS STEP IF YOU ARE UNABLE TO REMOVE THE DEVICE FROM THE APP.
If removal isn't possible, delete it by clicking "my device is broken" and then do the factory reset steps:

  • Hold the ON button for 12 seconds to reset

7. Dimming

  • Control dimming from 5-100% using either the app or wall dimmer

 

8. Manual override

  • If the light is OFF in the app, cycle power one time, the light will return to the previous ON state.