Eaton Logo
Go back to HALO Home page

Smart Outdoor Security Floodlight

1. Install the Smart LED floodlight in your desired location. (See enclosed instruction sheet.)

PLEASE NOTE: While HALO Home devices can be used on standard switches, they prefer constant power and then to be controlled wirelessly. To avoid accidental factory resets: install with HALO Home Controllers (Accessory Dimmer or Hardwired Multi-Room Scene Keypad).

When you power up the Floodlight it will:

  • Turns ON momentarily.
  • Turn OFF for approximately 4 seconds
  • Then turn ON at full brightness (100%), 4000K color temperature (CCT) and blink twice indicating it is ready to be claimed

Important:

  • Light blinks twice on power up if it remains unclaimed in the app
  • Light blinks once to indicate it has been claimed
  • It restores to the last saved brightness and color temperature levels on subsequent power cycles

If you have already registered for a Halo Home account, you may skip to step 4.


2. Download the HALO Home app to your smart mobile device.

 

3. Create a user account and validate via email

  • Enter your email address as your user account name.
  • Select a password of at least 8 characters from the mobile application “Register” screen.
  • Verify identity by clicking the link in your validation email.

 

4. Press “+” on the HALO Home App screen to add the floodlight

Note: At least one HALO Home compatible device will need to be installed and powered in order to add it to the device list.

 

5. The app will search for your installed, unclaimed lights

  1. Select the light and click “Add” to complete the pairing process
  2. The light blinks once to indicate it has been claimed

Note: The app works only when your HALO Home compatible device is powered and within approximately 40 feet depending on the Bluetooth range of your smart mobile device

 

Setting up a group

  1. At the top left, press the "  " menu icon and click on Groups to access the new grouping page.
  2. Tap the large plus sign in the center of the screen, or in the top right corner, to make your first group. Then enter a unique name for your group and tap “Done”.
  3. Touch and drag devices from the bottom of the screen towards the top of the screen to add them to your group. Repeat to add more and press next.
  4. That’s it! After your group is saved, you will be brought to the “Group Settings” menu.

 

Setting up a schedule

To set up a new schedule for a claimed device, follow these steps:

  1. Tap the "  " icon in the top left-hand corner
  2. Select the "Schedule" tab and click the “+” to set up a schedule
  3. Name your schedule
  4. Using the dial, set up your desired time & tap the days of the week you want the schedule active
  5. Press “Save” and then "Dismiss" after the confirmation notice pops up.
  6. Tap "Apply" in the top right corner and select the  Device/Group/Scene from the list
  7. Press “Save” to update and save your schedule

 

Reset to Factory Setting

ONLY DO THIS STEP IF YOU ARE UNABLE TO REMOVE THE DEVICE FROM THE APP.
If removal isn't possible, delete it by clicking "my device is broken" and then do the factory reset steps:

  • Using the wall switch, repeat this process 4 times:
    • OFF for 2 seconds
    • ON for 6 seconds.
  • The LED floodlight will flash twice after a successful reset

Dimming

  • The LED floodlight will dim from 100% to 5% using the mobile app

White Tuning

  • Use the mobile app to adjust color temperature (CCT) of the Bluetooth LED floodlights