Smart Outdoor Floodlight - Quick Start Guide
Your HALO Home Smart LED Floodlight expands your HALO Home Lighting to the outdoors. The Smart LED Floodlight provides HALO Home controlled security lighting where and when you need it. In this Quick Start Guide you will:
- Pair your installed HALO Home Smart LED Floodlight to the HALO Home App.
- Learn about additional features and information.
I. Pair Your Installed HALO Home Smart Floodlight to the HALO Home App
1. Install the Smart Floodlight in your desired location
(See enclosed instruction sheet)
Once powered your HALO Home Smart LED Floodlight will:
- turn ON momentarily
- turn OFF for approximately 4 seconds
- turn ON at full brightness (100%) & 4000K color temperature (CCT)
- flash twice to indicate that it is ready to be paired
2. Create your HALO Home Account
Download the HALO Home app and register >
Already a HALO Home user? Skip to the next step.
4. Add the HALO Home Smart Floodlight to the app
IMPORTANT! iPhone 11 Users. Having issues? Please read this>
Note: Make sure your mobile device’s Bluetooth is turned on and within 40’ of the Floodlight.
- Tap the " ☰" menu button.
- Navigate to "Devices" and tap the " + " icon.
(The app will scan for your installed, unpaired devices).
- Select "Floodlight" and click “Add” to complete the pairing process.
- The Smart LED Floodlight will blink once to indicate it has been paired.
Note: If the device firmware is outdated, an exclamation point will display on the device in the device list. Tap the exclamation point and following the onscreen instructions to update the device.
II. Additional HALO Home Smart Floodlight Features and Information
Now you can:
-
Add your light to a Group
-
Set up a Schedule
- Set up a Scene (Sets brightness and color temp where you need it.)
Override lighting manually (temporary)
To manually turn on the HALO Home Smart LED Floodlight without using the HALO Home App or accessories, cycle power to the light one time. The lighting will turn ON to its last known dim level until it receives the next HALO Home App, accessory, or voice command.
Reset the HALO Home Smart LED Floodlight to factory settings
ONLY DO THIS STEP IF YOU ARE UNABLE TO REMOVE THE DEVICE FROM THE APP.
If removal is not possible, delete it by clicking "my device is broken" and then do the factory reset steps:
To reset the HALO Home Smart Floodlight to factory settings:
- Using either a standard wall switch or the air-gap switch on an Accessory Dimmer cycle power to the HALO Home Smart LED Floodlight as instructed:
- Repeat this pattern 4 times:
- Turn OFF for 2 seconds
- Turn ON for 6 seconds
- Repeat this pattern 4 times:
- After a brief delay, the HALO Home Smart LED Floodlight will flash twice to indicate a successful reset.
HALO Home Smart Floodlight dimming
- The HALO Home Smart LED Floodlight will dim from 100% to 5%.
- Dimming must be done either with the app or with HALO Home dimmers and accessories.
Adjusting HALO Home Smart Floodlight color temperature
Use the mobile app to adjust color temperature (CCT) of your floodlight(s). (The HALO Home Smart LED Floodlight has a CCT range of 3000K to 5000K.)
Power cycle behavior
- An unpaired HALO Home Smart LED Floodlight will turn connected lighting ON to 100% and will flash twice if power is cycled
- A paired HALO Home Smart LED Floodlight will turn ON to the last known dim level if power is cycled.
(If lighting was OFF previous to the power cycle, lighting will turn ON when power is restored)