Eaton Logo
Go back to HALO Home page

Multi-Room Scene Keypad

1. Install the Scene Keypad in your desired location (See enclosed instruction sheet)

  • Once the keypad is installed properly:
    • Battery Powered: Ensure the LED indicator blinks after pressing the Power/Wake up button.
    • Hardwired: The LED should blink until claimed

If you have already registered for a Halo Home account, you may skip to step 4.


2. Download the Halo Home App to your smart mobile device

3. Register your account and validate

  • Enter your email address as your user account name.

  • Select a password of at least 8 characters from the mobile application "Register" screen.

  • Verify identity by clicking the link in your confirmation email.

4. Add the Scene Keypad to the app

A. Battery Version

  • Press the " ☰ " menu button in the upper left corner

  • Navigate to "Controllers". Then press the " + " button on the screen.

    - Battery Version: Select the “Battery Powered” tab (pictured below) And press the power button on the device to wake it up.

    - Hardwired Version: Select the “AC Powered” tab

  • Select the switch and press "Add". (It will take about 30 seconds for the process to complete.)

  • You can now associate it to a device.

 

Note: Stay in range. Your mobile device will need to be within 40' of the device when pairing.

5. Configure Keypad Buttons

  • In the menu under “Controllers”, select your Scene Keypad

  • Tap the “Pencil” icon on the key you are associating

  • Select the Device/Group/Scene you want to control and press “Save”.

  • Repeat this process for all four keys.
     

 

6. Using Your Keypad

  • Press (1-4) to turn ON that button's assigned Device/Group/Scene

  • Press UP/DOWN arrows to adjust the brightness

  • Double-tap same button to turn OFF assigned lighting

  • Double-tap Power/Wake up button to turn OFF all Devices/Groups/Scenes assigned to the entire keypad

 

RESETTING YOUR MULTI-ROOM SCENE KEYPAD

Remove the Scene Keypad unit from user account (using the app)

  1. Navigate to the Controller page in the app

  2. Select the Scene Keypad to open the controller settings screen

  3. Tap on "︙" menu in the top right corner

  4. Select the Remove option

  5. Battery Only: When prompted, press the Power/Wake-up button to complete the removal. 

  6. The process may take up to 30 seconds to complete.

After a successful reset:

  • Battery Powered - The LED indicator will stay on for 5 seconds then blink for 30 seconds 
  • Hardwired - The LED indicator will stay off for 7 seconds then begin blinking again

Alternate Reset Steps (Physical reset)

  1. Press the "1" button - 4 times

  2. Press the bottom "Power/Wake up" button - 4 times

  3. Press the "1" button - 4 more times

After a successful reset:

  • Battery Powered - The LED indicator will stay on for 5 seconds then blink for 30 seconds 
  • Hardwired - The LED indicator will stay off for 7 seconds then begin blinking again

IMPORTANT: If you physically reset your device - go to the app and remove the instance of the unit you have just physically reset.