Eaton Logo
Go back to HALO Home page

Create a Countdown Timer

Create Countdown Timer

  1. Tap the three vertical dots icon to the right of the device, or swipe from right to left on the device.
  2. Tap the Timer icon.
  3. Slide the hours and minutes sections to set the length of your countdown.
  4. Select On if you want your device to turn on, Off if you want your device to turn off, or Flash if you want it to flash when the countdown finishes.
  5. Tap Start to start your countdown.
  6. The countdown will begin.
  7. When the countdown ends, your lighting device will execute the command you gave it and and you will receive an in-app notification.