Eaton Logo
Go back to HALO Home page

Add Smart LED Motion Sensor Flood to Your Account

Note: This product contains a smart LED floodlight and a smart motion
sensor; each can be controlled separately and associated with separate
devices. Therefore, each needs to be claimed separately.

Add the Floodlight to Your Account

  1. Navigate to the Devices index from the main menu.
  2. Press “+” on the index screen to add your Floodlight.
  3. Make sure the AC Powered tab is active on the screen.
  4. Select the Floodlight you wish to add and tap Add on the bottom right of the screen.
  5. The light blinks once to indicate it has been claimed. It restores the saved dimming and CCT levels on subsequent power cycles.
  6. Once claimed to your account, you will be presented with the Device Configuration screen where you can name your Floodlight, take a picture of it, and set dimming and CCT preferences.

 

Add the Motion Sensor to Your Account and Associate with Lighting Devices

  1. Navigate to the Devices or Controllers indexes from the main menu.
  2. Press “+” on the index screen to add your Motion Sensor.
  3. Make sure the AC Powered tab is active on the screen.
  4. Select the Sensor you wish to add and tap Add on the bottom right of the screen.
  5. Once claimed, the blue LED indicator on the bottom of the motion sensor will blink twice and then remain on to indicate it has been claimed.
  6. The Controller Settings screen will appear for your motion sensor. Press Associate or Tap to select.
  7. Select the Device or Group to be controlled by your motion sensor and press Save.

Note: Only one Device or Group can be selected. To control multiple Devices, create a Group from the Groups index in the main menu, then return to the Controller Settings screen to associate the motion sensor to that group.

 

Adjust Your Motion Sensor Settings

  1. Edit the name of your motion sensor.
  2. Activate or deactivate your motion sensor. Turning this off deactivates the sensor, allowing you to control the floodlight or other associated devices manually.
  3. Change which HALO Home devices are controlled by the motion sensor.
  4. Define how the associated device or group reacts to a motion event, and for how long.
  5. Activate or deactivate Standby: how a device reacts once the duration time has expired after a motion event.
  6. Define how the associated device or group reacts in Standby mode, and for how long.
  7. Set the sensitivity level of the motion sensor.
  8. Set the sensitivity level of the photocell within the motion sensor.

Note: Be sure to press Save after making changes to the settings to ensure any changes are retained.

 

Motion Event and Standby Settings

  1. Dimming: Set the dim level activated by a motion event. The LED floodlight can dim from
    100% to 5%.
  2. Color Tuning: Set the color temperature (CCT) activated by a motion event, or select one of the presets. The LED floodlight has a CCT range of 3000K to 5000K.
  3. Duration: Set the length of time these settings will remain in effect when motion is detected.

Note: This countdown timer continually resets as additional motion events occur.

 

Motion Sensitivity and Test Mode

  1. Adjust motion sensitivity, or range, by using the slider or the preset buttons.
  2. Activate Test Mode to test the range of the motion sensor, day or night, as you make adjustments to the sensitivity. The associated device or group will turn on for a few brief seconds between motion events. Deactivate this mode after choosing the sensitivity that works best for your application.

 

Photocell Sensitivity

  1. Adjust the photocell sensitivity by using the slider or the preset buttons.
  2. The motion sensor only activates fixtures at night. Photocell sensitivity determines how dark it needs to be for the motion sensor to begin doing this; choose low sensitivity to have devices wait until it is very dark at night to begin activating, while stopping earlier in the morning at dawn. A high sensitivity will activate the motion sensor as soon as dusk begins, and keep it active until later in the morning.