Eaton Logo
Go back to HALO Home page

Create, Modify, and Remove a Schedule

Create a Schedule

  1. Navigate to the Schedules page from the main menu.

  2. Tap the "+" icon on the top right of the index screen to create a new schedule.

  3. Name your new schedule

  4. Select your schedule type: On/Off, On, Off
  5. On the schedule screen, move your finger around the 24-hour clock to set the ON and OFF times. There are a few helpers on this screen too:

    • The Sunrise icon sets a schedule to turn ON at sunrise and OFF at sunset.*

    • The Sunset icon sets the schedule to turn ON at dusk and OFF at dawn.*

    • The Random icon creates random ON and OFF times. You can use this feature to make it appear you are home when you are on vacation.

      *You must have location services active on your mobile device for this feature to function properly.

  6. Select the days of the week you want your new schedule to execute.

  7. Tap Save at the top right of the screen.

  8. HALO Home will save your new schedule. Select Dismiss to return to the schedule screen.

  9. Select the Schedule you would like to associate to devices, groups or scenes.

  10. To apply your new schedule to a device, group of fixtures, or a scene, swipe left on the selected schedule and tap Apply at the top right of the screen.

  11. Select the Devices/Groups/Scenes you want this schedule to control

  12. Tap Save at the top right.

  13. HALO Home will assign your schedule.

  14. You schedule is now ready to execute at the appropriate times.

Note: If a Group is applied to a Schedule, devices belonging to the Group will not be listed or available for selection under Devices.

 

Modify a Schedule

  1. Navigate to the Schedules page from the main menu.

  2. Slide the list item left and tap Edit on the Schedule you wish to modify.

  3. Use the same schedule controls to edit the schedule to your liking.

  4. Press Save at the top right of the screen.

  5. HALO Home will save your modified schedule.

  6. Your modified schedule is not ready to execute at the modified times.
     

Remove a Schedule

  1. Navigate to Schedules page from the main menu

  2. Tap and swipe left on the 3 dot button on the schedule you want to delete

  3. Now the drawer menu on that schedule icon shows the Apply, Edit & Delete options

  4. Tap on the Delete option on the drawer menu

  5. Tap "Delete" on the popup asking for confirmation

  6. When complete you will see a schedule deleted confirmation message

Note: Make sure that the devices to which schedule is assigned is powered ON to successfully remove the schedule from devices