Eaton Logo
Go back to HALO Home page

Can more than one person in my household control my lighting devices?

Yes, more than one person in your household can control your lighting devices.
Multiple users in a location can have the HALO Home app on their mobile phones as long as each person is using the same account credentials.

NOTE: A "sparse network" can be created if there are more phones logged into the app than the number of devices powered ON.
(If, for example, multiple phones need to use HALO HOME app - and there is only one light in account - only one user should use the app at a time)